Technical FAQs

Ask a Question

9998L Coils and Inrush

Issue:
What is the inrush and sealed VA ratings for the 9998L coils?

Product Line:
Lighting contactors, accessories, coils

Environment:
9998 Replacement parts

Cause:
To assist in calculating the inrush and sealed VA ratings.

Resolution:
For 2 - 6 poles the rating is 150VA inrush and 30VA sealed.
For 8 - 12 poles the rating is 180VA inrush and 35VA sealed.

Was this helpful?
What can we do to improve the information ?