Technical FAQs

Ask a Question

9013GSG1J29

Issue:
What is 9013GSG1J29

Product Line:
9013G Pressure switch

Environment:
US product

Cause:
9013GSG1J29 is a switch in use which is set to a higher pressure than what it is specified for and not valid in ordering system.

Resolution:
This switch was manufactured for bulk sale to one customer but never put into system.  It can be replaced with 9013GHG1J29.

Was this helpful?
What can we do to improve the information ?