Technical FAQs

Ask a Question

Can the main breaker in EZM31600GCBC be adjusted down to 1000A?

Issue:
Adjustable trip range

Product Line:
EZM Main Breaker

Environment:
1600A Main Breaker

Cause:
Different long time trip setting required

Resolution:
The RGF36160U31A main breaker can be adjusted, but has an A rating plug with .60 and .63 mulitpliers, which would adjust to 960A or 1008A as the closest values to 1000A. If the A rating plug was replaced with an H rating plug, part number S48840, a trip setting of 992A could be achieved by setting the H rating plug to the .62 multiplier.  
Was this helpful?
What can we do to improve the information ?