Technical FAQs

Ask a Question

LAF263501230 Suffix

What does the suffix -1230 mean on an LAF/LAL Circuit Breaker? 

Product Line:
Legacy L Frame Circuit Breakers.

Applies to LAF/LAL  type circuit breakers.

There is a need for a special code for 2 combinations of accessorie for the LAF breaker.

Suffix 1230 is a 120 to 240 volt shunt trip plus special calibrations on the Magnetic trip feature of the breaker.
Was this helpful?
What can we do to improve the information ?