Technical FAQs

Ask a Question

Does Square D offer a fusible double throw safety switch?

Issue:
Selection

Product Line:
Double Throw Safety Switch

Environment:
Product selection

Cause:
Selection

Resolution:
Yes, we do but only in 30A - 100A, 2 pole (240V,100A only) and 3 pole (240V or 600V, 30A - 100A) construction; in Type 1 or Type 3R enclosures.
Was this helpful?
What can we do to improve the information ?