Technical FAQs

Ask a Question

What are the repair parts for a QO612L100RBCU, Series G02 (or G2), Load Center?

ISSUE:
Current design repair parts 

PRODUCT LINE:
QO Load centers

ENVIRONMENT:
Repair parts

CAUSE:
Maintenance.

RESOLUTION:
Only the parts listed below are considered field replaceable.
Cover - 4055342450  
Interior assembly - 4055324950   
Interior Trim - 4055309302  
Neutral Bonding Screw - 4028329751 (bag assembly with bonding screw, trim screws, service disconnect and Main label)  
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142717161  


Was this helpful?
What can we do to improve the information ?