Technical FAQs

Ask a Question

Why are the menus scrambled or displaying the wrong data in menu 1.14 using the water solutions card on the ATV61 drives?

Issue:
Why are the menus scrambled or displaying the wrong data in menu 1.14 using the water solutions card on the ATV61 drives?
Product Line:
Altivar ATV61 with the Water Solutions Card VW3A3503
Environment:
All
Cause:
Destage menu are scrambled or mixed up in menu 1.14 or you may see menus parameter from one menu showing up misplaced in another menu.
Resolution:
If using an external power supply do the following: ;
1.) Wire the external power supply to P24 and 0V so you power up the water solution card and the Main control board at the same time.
2.) Do a factory reset on the VFD
3.) Before any programming of the VFD, set the Inlet Transducer Maximum (Inlet TX Max) to the maximum value (32765) in menu 1.14 Water Solut. – Expansion -Sensors

 
Was this helpful?
What can we do to improve the information ?