Technical FAQs

Ask a Question

What are the repair parts for a QO13040M200GRB, Series S02 (or S2), Load Center?

Issue:
Current design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4056317550   
Interior Trim - 4056313501
Interior Assembly - 40559-211-51    
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2200VH
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142217101
Outdoor Cover Latch - 4056314701
Outdoor Cover Latch Rivet - 2410212160
Main Circuit Breaker and Main Lugs Keps Nuts - 2342702001
Was this helpful?
What can we do to improve the information ?