Technical FAQs

Ask a Question

What are the repair parts for a QO132M150, Series S1 (or S01), Load Center?

Design repair parts

Product line:
QO load centers

repair parts


Only the parts listed below are considered field replaceable.
Cover - QOC40UF/S
Interior Assembly - 40559-212-53  (interior assembly does NOT include the Main breaker, see main breaker below)  
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2150VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main Circuit Breaker and Main Lugs Keps Nuts - 2342702001
Was this helpful?
What can we do to improve the information ?