Technical FAQs

Ask a Question

What is the impedance of the analog input AI1 on the ATV312?

Issue:
Analog input one impedance of the ATV312

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
The impedance of AI1 on the ATV312 is 30K ohms

Was this helpful?
What can we do to improve the information ?