Technical FAQs

Ask a Question

Can the XALK188H7 be keyed differently?

Can the XALK188H7 be keyed differently?

Product Line:
22mm control station

XALK control station

Maintenance and product feature

The XALK188H7 does not come with the option for a different key.
Suggest ordering the keyed operator, contact blocks and enclosure seperately - the keyed operator will alloy for different keys.
For the operator our options are the ZB5AS94410, ZB5AS94412, ZB5AS94414, and the ZB5AS94420.
The enclosures part number is XALK01H7 and the contact block will be part number ZENL1121.

Was this helpful?
What can we do to improve the information ?