Technical FAQs

Ask a Question

Does 8910DPA93 have boxed lugs or quick connect?

ISSUE:
Does 8910DPA93 have boxed lugs or quick connect?

Product Line:
Definite Purpose Contactors

Environment:
8910DPA93, 40A - 90A

Cause:
Need to know type of termination.

RESOLUTION:
Per current 8910 catalog, it has box lugs. This device also has double stab provisions for using a quick-connect termination.

 
Was this helpful?
What can we do to improve the information ?