Technical FAQs

Ask a Question

Is there an option card that allows you to set the date and the time in an AC Drive?

Issue:
Is there an option card that allow you to set the date and the time in an AC Drive?

Product line:
ATV61, ATV71

Environment:
All models, all serial numbers 

Cause:
Need to set time in AC Drive.

Resolution:
IMC Card VW3A3521S0  and/or CIC Card VW3A3501  permit this even if not being used to control the drive. These option cards do require an external +24 volt power supply.
Was this helpful?
What can we do to improve the information ?