Technical FAQs

Ask a Question

Is a white cover available for the HOM30L125C load center?

Issue:
Product availability

Product Line:
HOMELINE load center

Environment:
Non standard cover

Cause:
Customer preference

Resolution:
Yes, it is. The HOM30L125C will come with the standard gray (ANSI-49) cover provided. To purchase a separate white cover, order HOMC30U125CW.

Was this helpful?
What can we do to improve the information ?