Technical FAQs

Ask a Question

Is a neutral provided with a HU364AWK safety switch?

Issue:
Product feature

Product Line:
Heavy Duty Safety Switch

Environment:
Selection

Cause:
Understanding what components are provided

Resolution:
No, it is not. For current F06 design series, order SN20A (Al/Cu) or SN20C (Cu Only) separately for field installation. For a 200% neutral application, order two neutral kits and SN20NI neutral jumper kit.
Was this helpful?
What can we do to improve the information ?