Technical FAQs

Ask a Question

What is a neutral position as on the 9007C68T10, or any other limit switch?

Define neutral position on a limit switch or sensor.

Product Line:
Limit Switches, products in 9006CT1007 Sensor catalog.

Products sold and used in the United States


As defined by the Sensor Master Catalog 9006CT1007,

"Lever operated switch with a minimum of two contacts. One contact
changes state only when the lever moves CW. The second contact
changes state only when the lever moves CCW. Used when the direction
of a part or cam needs to be identifi ed. This can be used for an indication
of the direction of the cam, such as “up, off, down” or “forward,
off, reverse”."

neutral position, limit switch, 9007, 9007C, 9007A, 9007MS, 9007ML, XCMD, XCMN, XCKD, XCKP, XCKT, XCDR, XCPR, ZCE, ZCY, ZCD, ZCMC, ZCMD, ZCP, ZCPE, XCKN, XCNR, XCKS, XCKJ, XCKL, 9007T, 9007FT,

Was this helpful?
What can we do to improve the information ?