Technical FAQs

Ask a Question

Can a load center interior be removed from the enclosure?

Issue:
Product feature

Product Line:
Load Centers

Environment:
QO, HOMELINE and TRILLIANT

Cause:
Various reasons to remove the interior

Resolution:
Yes, the interior base assembly can be removed from any QO, HOMELINE and/or TRILLIANT load center.

Was this helpful?
What can we do to improve the information ?