Technical FAQs

Ask a Question

Can a HOM40M200C or HOM40M200VP be converted from a 200A main breaker panel to 100A?

Issue:
Main breaker conversion

Product Line:
Homeline Load Center

Environment:
Homeline Load Center Main Breaker

Cause:
Needs the higher number of circuits, but with a lower amperage main breaker

Resolution:
Yes, the QOM2200VH main breaker that would be provided factory installed can be changed out with a 100A QOM2100VH.
Was this helpful?
What can we do to improve the information ?