Technical FAQs

Ask a Question

Are lugs provided on the EZM32000CBU?

Issue:
Lug data

Product Line:
EZM Meter Pak

Environment:
EZM Main Circuit Breakers and Main Fusible Switches

Cause:
Understanding for factory installed features

Resolution:
No, this unit comes only with lug landing pads for field installation of customer (or utility company) provided lugs. Refer to the approval drawing available in the Technical Library for a list of acceptable lugs. 
Was this helpful?
What can we do to improve the information ?