Technical FAQs

Ask a Question

Where can I download the Drives configuration APP software for Altivar drives?

Issue:
Where can I download the Drives configuration APP for Altivar drives?

Product Line:
Altivar ATV212, ATV61, ATV71

Environment:
All

Cause:
Drives configuration APP

Resolution:
https://itunes.apple.com/us/app/drives-soft-starts-visual/id579066980?mt=8

Please note that this software APP  will not work with the Iphone it will only work with the IPAD.

If you are using the 30 pin connector  you will need to make sure its an official Apple product.

 

Was this helpful?
What can we do to improve the information ?