Technical FAQs

Ask a Question

What is the master password to reset the ATV12 drives?

Issue:
What is the master password to reset the ATV12 drives?

Product Line:
Altivar ATV12

Environment:
All

Cause:
Password has them locked out of the drive.

Resolution:
The master password is 2663 to unlock the drive.
 

Was this helpful?
What can we do to improve the information ?