Technical FAQs

Ask a Question

What is the HP rating for H82344?

Issue:
Horsepower rating

Product Line:
Double Throw Safety Switch

Environment:
200A DT Switch

Cause:
Confirm HP rating

Resolution:
The switch carries a 15 HP rating @ 480Vac. Do not use on a motor load application over 15 HP @ 480Vac.
Was this helpful?
What can we do to improve the information ?