Technical FAQs

Ask a Question

Is the EZM11200GCBU suitable only for bottom feed?

Issue:
Confirming design

Product Line:
EZM Meter-Pak Meter Centers

Environment:
EZM 1200A Main Breaker and Main Fusible Switch Units

Cause:
Confirmation of service feed, overhead or underground

Resolution:

Yes, that is correct. This device can only accept the service feed from the bottom (underground service feed).

Was this helpful?
What can we do to improve the information ?