Technical FAQs

Ask a Question

What are the repair parts for a QO816L100DSCU, Series G4, Load Center?

Current design repair parts

Product Line:
QO Load centers

Repair parts



Only the parts listed below are considered field replaceable.
Cover - 40553-453-51  
Interior Assembly - 4055325050
Neutral Bonding Screw ONLY  - 4020506903
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
NOTE: Labeling is not supplied on the replacement cover and the cost of the replacement cover may be close to, or exceed, the cost of a new device. You may want to consider buying a new device and use the new cover on the existing device.
Was this helpful?
What can we do to improve the information ?