Technical FAQs

Ask a Question

What are the repair parts for a QO816L100DFCU, Series G4, Load Center?

Issue:
current design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable.
Cover - 4055345250   
Interior Assembly - 4055325050   
Neutral Bonding Screw ONLY - 4020506903 
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
Was this helpful?
What can we do to improve the information ?