Technical FAQs

Ask a Question

Is the J250DS also available in Type 316 stainless steel?

Issue:
Type of stainless steel

Product Line:
Circuit Breaker Enclosure

Environment:
Type 4X application

Cause:
Confirming type of stainless steel used.

Resolution:
Yes, if Type 316 stainless steel is required, order J250SS. 
 
Was this helpful?
What can we do to improve the information ?