Technical FAQs

Ask a Question

What is the busbar rating for SC1624M125S?

Issue:
Busbar rating

Product Line:
Combination Service Entrance Device

Environment:
Ratings of busbars

Cause:
PV application

Resolution:
The busbar rating is equal to the maximum mains amperage noted on the labeling, which is 125A on the SC1624M125S.



Was this helpful?
What can we do to improve the information ?