Technical FAQs

Ask a Question

Can a P1200R circuit breaker enclosure be mounted horizontally?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Environment:
Installation

Cause:
Orientation of installation

Resolution:
No, the NEMA Type 3R circuit breaker enclosures that have not been tested, nor listed for horizontal mounting. The enclosure can only be mounted vertically.

Was this helpful?
What can we do to improve the information ?