Technical FAQs

Ask a Question

What is the maximum voltage rating for the 82344 double throw safety switch?

Issue:
Electrical ratings

Product Line:
Double Throw Switch

Environment:
200A Double Throw

Cause:
Assure applying correctly

Resolution:
This double throw switch is rated for use on 480Vac or 250Vdc maximum.

Was this helpful?
What can we do to improve the information ?