Technical FAQs

Ask a Question

ATV312, are these drives suited to be highpot?

Issue:
ATV312, are these drives suited to be highpot test?

product Line:
ATV312

Environment:
All 

Cause:
None.

Resolution:
It is not recommended to High Pot the VFDs. It may damage the VFDs.
Was this helpful?
What can we do to improve the information ?