Technical FAQs

Ask a Question

Is there a communication card available to support RSTP (Rapid Spanning Tree)?

Issue:
Is there a communication card available to support RSTP (Rapid Spanning Tree)?

Product Line:
ATV61/71

Environment:
All range, All serial number

Cause:
None

Resolution:
Currently, there is no card available to support RSTP. It is in the works but there is no timeline available.

Was this helpful?
What can we do to improve the information ?