Technical FAQs

Ask a Question

What encoder can be used to get emulation output?

Issue:
What encoder can be used to get emulation output?

Product Line:
ATV61/71

Environment:
All range, All serial number

Cause:
None

Resolution:
Need to use ATV71...N4383 drive with VW3A3411 encoder option card.

Was this helpful?
What can we do to improve the information ?