Technical FAQs

Ask a Question

What is the line supply tolerance on the 575vac ATV71/61.........Y drives?

Issue:
What is the line supply tolerance on the 575vac  ATV71/61.........Y drives? 

Product Line:
ATV71/61 ....Y

Environment :
575VAC only

Cause
Needs to know what the line supply tolerance voltage is on the 575vac drives.

Resolution:
500V -15% and 690V +10%
 
Was this helpful?
What can we do to improve the information ?