Technical FAQs

Ask a Question

What are the specs, ratings and accessories for the NSYTRV43PE, NSYTRV44PE grounding type terminal block?

Issue:
Where can specs, ratings and accessories be found on the new Linergy line terminal block NSYTRV43PE, NSYTRV44PE?

Product Line:
Linergy TR Screw terminal blocks.

Environment:
Linergy TR NSYTRV43PE, NSYTRV44PE Double deck grounding type terminal block.

Cause:
To clarify the differences for the new line of terminal blocks compared to the old AB1 terminal blocks.

Resolution:
All of the specifications, ratings, and accessories for this terminal block are found on page 28 in the LINERGY CATALOG 9080CT1301.  See attached.

Was this helpful?
What can we do to improve the information ?