Technical FAQs

Ask a Question

How Do I Setup an MPPT60 - 150 without an SCP or Combox

Issue:
How to get to advanced settings on MPPT60 without SCP

Environment:
XW MPPT60-150 without a System Control Panel or Conext Combox

Product Line:
MPPT60 - 150

Resolution:
Go to Display Menu, Select Advanced under Display Mode.  After that all the settings highlight in gray will become available.



Cause:
Some installations may have the MPPT60-150 installed standalone, or simply without any of the modular configuration accessories.  Since the MPPT60-150 has its own interface, commissioning can be done without an SCP or Conext Combox
Was this helpful?
What can we do to improve the information ?