Technical FAQs

Ask a Question

What are the specs, ratings and accessories for the NSYTRV162 terminal block?

Issue:
Where can specs, ratings and accessories be found on the new Linergy line terminal block NSYTRV162?

Product Line:
Linergy TR Screw terminal blocks.

Environment:
Linergy TR NSYTRV162, NSYTRV122BL

Cause:
To clarify the differences for the new line of terminal blocks compared to the old AB1 terminal blocks.

Resolution:
All of the accessories for this terminal block is found on page 21 in the LINERGY CATALOG 9080CT1301.  See attachment.

Was this helpful?
What can we do to improve the information ?