Technical FAQs

Ask a Question

Micrologic 5.0P 6.0P 5.0H 6.0H trip units are not recording trip history events.

Issue:
Not recording any of the trip values in trip history, only says Integr Inst and no date

Product Line:
Micrologic 5.0P 6.0P 5.0H 6.0H trip units

Environment:
Powerpact P, R frame,  and Masterpact NT NW

Cause:
Unpowered trip unit or primary injecting breaker while FFTK or HHTK plugged in to the trip unit

Resolution:
The trip history will not record values on an unpowered trip unit (not externally powered with a 24Vdc power supply), after a breaker trip, the trip unit turns off and does not have time to record the trip history information.
The end user will need to add 24Vdc to the trip unit in order to utilize this function, on trip unit terminals F2 (+) and F1(-).

The trip history will not record values while using the FFTK (Full Function Test Kit) or HHTK (Hand Held Test Kit) to test or inhibit.
Plugging in the FFTK or HHTK just to power the trip unit, while primary injection testing, will allow it to recorded a trip history.
Was this helpful?
What can we do to improve the information ?