Technical FAQs

Ask a Question

Can an H frame PowerPact breaker be used in J225X enclosure?

Issue:
Enclosure selection

Product Line:
Circuit Breaker Enclosure

Environment:
Type 9

Cause:
Proper application of enclosure

Resolution:
The enclosure is marked for use with JDL and JGL breakers only.
The maximum SCCR is 65 kAIR @ 240Vac, 25 kAIR @ 480Vac, 18 kAIR @ 600Vac.

Was this helpful?
What can we do to improve the information ?