Technical FAQs

Ask a Question

What are the repair parts for a HOM816M150FTRB, Series S03, load center?

Issue:
current design repair parts

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Cover - 4056317550 (Includes hinges attached to left side of cover)            
Cover Mounting Screw - 2142217101 (2 required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056313301K              
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056508051 (interior assembly does not include the main breaker, see below main breaker) 
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM2150VH
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?