Technical FAQs

Ask a Question

Plug-in base vertical termination orientation when factory installed. Suffix TC.

Issue:
Plug-in base vertical termination orientation when factory installed.  Suffix TC.

Product Line:
Powerpact H, J and L

Environment:
Plug-in base terminal orientation

Cause:
Needed for designing equipment bussing.

Resolution:
When looking at the top of the plug-in base, the vertical terminals are left facing.   See page 3 of the attached marked up installation instructions.
Was this helpful?
What can we do to improve the information ?