Technical FAQs

Ask a Question

Does the 9001KYG1 have a Replacement Front Cover

Issue:
Can the front half of 9001KYG1 be ordered separately?

Product Line:
9001K Enclosures/Control Stations

Environment:
Maintenance/replacement 

Cause:
Front half of station may need to be replaced without replacing back half.

Resolution:
The 9001KYG1 must be ordered as one complete unit. The front cover is not available as a separate component.

Was this helpful?
What can we do to improve the information ?