Technical FAQs

Ask a Question

Is the QO1HPL UL Listed?

Issue:
UL Listing

Product Line:
Circuit Breaker Accessory

Environment:
Standards

Cause:
Understanding standards approval

Resolution:
Yes, it is UL Listed in File E84625 as a Circuit Breaker Accessory. The UL mark is provided on the package labeling but not directly on the accessory. 
Was this helpful?
What can we do to improve the information ?