Technical FAQs

Ask a Question

Is the fuse mounting hardware required to mount a Class L fuse in a 800A or 1200A Heavy Duty Safety Switch provided with the switch?

Issue:
Installing Class L fuses in an 800A safety switch

Product Line:
800A 1200A Heavy Duty Safety Switches

Environment:
Distribution Equipment Safety Switch

Cause:
Class L fuses are bolt on, so the proper mounting hardware is required
 
Resolution:
Yes, the mounting bolts, washers and nuts are provided to connect the Class L fuses in the switch. The hardware will be included on the connector pads where the fuses will be mounted.
Was this helpful?
What can we do to improve the information ?