Technical FAQs

Ask a Question

What are the repair parts for a HOM1624M225RB, Series S03 load center?

Issue:
Current design repair parts

Product Line:
Homeline Load Centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable.
Cover - 4056317450  
Cover Mounting Screw - 2142217101 (2 Required)         
Interior Trim with Labels - 4056354201K      
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056549751 (interior assembly does not come with the main breaker, see below main breaker)  
Main Breaker - QOM2225VH
Neutral Bonding Screw - 4028345850K      
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?