Technical FAQs

Ask a Question

What are the repair parts for a HOM4060M200RB, Series S03 load center?

Curren design repair parts

Product Line;
Homeline load centers

Repair parts



Only the parts listed below are considered field replaceable.
Cover - 4056317250 (Includes hinges attached to left side of cover)         
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056314202K                 
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056591351 (interior assembly does not include the main breaker, see below main breaker) 
Main Breaker - QOM2200VH
Neutral Bonding Screw - 4028345850K
Note: Cover does not have labels applied.
Was this helpful?
What can we do to improve the information ?