Technical FAQs

Ask a Question

Is there a Retaining Kit available to backfeed a 2 pole QO branch breaker in a QO24L70F?

Issue:
Product selection

Product Line:
QO Load Center

Environment:
QO Load Center accessories

Cause:
Backfeeding a branch breaker

Resolution:
 No, there is not. In a 2 space load center, there would be no reason to backfeed a 2 pole branch circuit breaker. Since there are only 2 spaces in this load center, so there would be no space for other branch breakers for the backfed breaker to feed.
Was this helpful?
What can we do to improve the information ?