Technical FAQs

Ask a Question

How do you change the outputs on the Zelio REG24 Temperature Controllers to control heating or cooling?

Issue:
How do you change the outputs on the Zelio REG24 Temperature Controllers to control heating or cooling?


Product Line:
Zelio Temperature Controllers with part numbers starting with REG24

Environment:
Temperature Controllers sold and used in the United States

Cause:
The temperature controller default is to control heating on Output 1.

Resolution:

To change the output type to the desired function:

Accessing the parameter
1.     Press the SEL key until Ch 1 is displayed.
2.     Press the Down Arrow key until Ch 2 is displayed.
3.     Press the SEL key.
4.     Press the Down Arrow key until rEv is displayed.
5.     Press the SEL key.
6.     Change the value from the default  using the Arrow keys to:

Please note Reverse is Heating and Normal is Cooling



 rEv Control output 1 Control output 2
 rv-- Reverse -
 no-- Normal -
 rvno Reverse Normal
 norv Normal Reverse
 rvrv Reverse Reverse
 nono Normal Normal


 


Was this helpful?
What can we do to improve the information ?