Technical FAQs

Ask a Question

What are the repair parts for a HOM2040M200RB, Series S03, load center?

Issue:
Previous design repair parts

Product Line:
Homeline load centers

Evnironment:
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable.
Cover - 4056317550 (Includes hinges attached to left side of cover)     
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056313701K       
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056508551 (Obsolete, NLA, order HOM2040M200PRBI)          
Main Breaker - QOM2200VH
Neutral Bonding Screw - 4028345850K
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?