Technical FAQs

Ask a Question

How do you select the input type (analog, thermocouple, PT100, RTD) on the Zelio REG48 or REG96 Temperature Controllers?

Issue:
How do you select the input type (analog, thermocouple, PT100, RTD) on the Zelio REG48  or REG96 Temperature Controllers?

Product Line:
Zelio Temperature Controllers with part numbers starting with REG48 and REG96

Environment:
Temperature Controllers sold and used in the United States

Cause:
By default, the input type is 2 (Type J thermocouple).

Resolution:

Accessing the parameter
1.     Press the SEL key until Ch 1 is displayed.
2.     Press the Down Arrow key until Ch 6 is displayed.
3.     Press the SEL key.
4.     Press the Down Arrow key until PvT is displayed.
5.     Press the SEL key.
6.     Change the value from the default  to one of the following using the Arrow keys.

Value: Input Type

0 (JPT 100 Ω )
1 (PT 100 Ω )
2 (J)
3 (K)
4 (R)
5 (B)
6 (S)
7 (T)
8 (E)
9 (no function)
10 (no function)
11 (no function)
12 (N)
13 (PL-2)
14 (no function)
15 (0 V...5 V / 0 mA...20 mA)
16 (1 V...5 V/4 mA...20 mA)
17 (0 mV...10 V)
18 (2 V...10 V)
19 (0 mV...100 mV)

 


Was this helpful?
What can we do to improve the information ?