Technical FAQs

Ask a Question

What are the repair parts for a HOM816M125RB, Series S03, load center?

Current design repair parts

Product Line:
Homeline load centers

Repair parts



Only the parts listed below are considered field replaceable.
Cover - 4056317850 (Includes hinges attached to left side of cover)  
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056312702K          
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056507251  (interior assembly does not come with the main breaker, see below main breaker) 
Main Breaker - QOM125VH
Neutral Bonding Screw - 4028345850K
Note: Covers do not have labels applied.
Was this helpful?
What can we do to improve the information ?